Skip to main content
AKUMA.7
Visitor II
September 7, 2022
Question

what is the GPIO read speed of IDR for stm32L-152RE ?

  • September 7, 2022
  • 2 replies
  • 660 views

Hello, 

Basically i am trying to get data at GPIO with inc with clk. The clk is used as a interrupt. The speed of interrupt is 500KHz.

Here i am able to detect each intrrupt but i am missing the data at GPIO and not able to get the same data every time. I have tried the multiple method with log pulse but not getting recognised.

Here is the code:

Method 1:-

 void EXTI15_10_IRQHandler(void)

{

 // EXTI line interrupt detected

 if (__HAL_GPIO_EXTI_GET_IT(GPIO_PIN_13) != RESET)

 {

  __HAL_GPIO_EXTI_CLEAR_IT(GPIO_PIN_13);

 data = ((GPIOB->IDR & GPIO_PIN_1)>>1); // here is the data varible to read GPIO

 }

}

Method 2:-

void EXTI15_10_IRQHandler(void)

{

 // EXTI line interrupt detected

 if (__HAL_GPIO_EXTI_GET_IT(GPIO_PIN_13) != RESET)

 {

  __HAL_GPIO_EXTI_CLEAR_IT(GPIO_PIN_13);

  i_flag = 1;

 }

}

void main(void)

 {

 while (1)

 {

 if(i_flag != 0)

 {

 i_flag = 0;

 temp = ((GPIOB->IDR & GPIO_PIN_1)>>1);

 data[a] = (uint8_t*)temp;

 a ++;

  }

  }

 }

  

The both way are not working and I don't have clue about it. Please suggest if it can be solved.

I have seen many similar issue on community but did not get solution.

    This topic has been closed for replies.

    2 replies

    Piranha
    Principal III
    September 7, 2022
    1. ST employee.
    2. Added a ridiculous "GPIO Data Miss At Interrupt" tag to the forum.
    3. Does a nonsense like 500 kHz interrupts on EXTI, especially on 32 MHz CPU.
    4. Code posted not in a Code Snippet.
    5. Variable definitions are not shown.
    6. Most likely data/i_flag variables are not defined as volatile.
    7. Lack of a basic C programming skills (casting the temp variable as a pointer).
    8. Uses __HAL_***_IT() macros where __HAL_***_FLAG() macros must be used.
    9. Combines HAL with register programming for no reason.
    10. Not capable of using Google, Stack Overflow or searching this forum.

    Is this a joke?

    @Laura C.​, at least remove that "useful" tag from the system...

    Tesla DeLorean
    Guru
    September 7, 2022

    500 KHz? so you've got perhaps 64 cycles to work with. How many just stacking/unstacking context?

    Perhaps you'd do better using DMA and pulling the 16-bit wide IDR into a buffer at the rate you want, and then pick through it at your leisure?

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..