cancel
Showing results for 
Search instead for 
Did you mean: 

What is the difference between STM32L151CBU6 and STM32L151CBU6A? Can they be interchangeably used?

igamoso
Associate III

What is the difference between STM32L151CBU6 and STM32L151CBU6A?

Can they be interchangeably used?

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
GLASS
Senior

Some year ago we tried to replace stm32l151rct6 by stm32l151rct6A.

We detected instability, may be due to pll default at startup.

We were surprised that A ref was very quickly NRFND​ (Not Recommanded For New Design).

May be it confirm that A ref was a bad try and was abandoned...

Now all stm32l1 are NRFND.​

May be give a look to L4 or U5...

Not sure that it is pin to pin compatible for your design (you must check), but for sure that​ need rework for SW.

Peter BENSCH
ST Employee

There is a technical note TN1176 describing the migration from e.g. the (older) STM32L15xx6/8/B to the (newer) STM32L15xx6/8/B-A and the differences.

Yes, both are already on NRND, but will still be produced until the end of 2031. Nevertheless, as @GLASS​ noted, it makes sense to switch to another family.

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.