2008-06-09 03:32 AM
What is FLITF in Cortex-M3 architecture?
2011-05-17 03:36 AM
Quote:
On 09-06-2008 at 14:03, Anonymous wrote: In the system architecture block diagram of Cortex-M3 there is a block called FLITF between Flash and Cortex core. What does FLITF stands for and what is its functionality? Flash memory interface, it has the logic/buffers to perform read/write operations on the FLASH2011-05-17 03:36 AM
In the system architecture block diagram of Cortex-M3 there is a block called FLITF between Flash and Cortex core. What does FLITF stands for and what is its functionality?