cancel
Showing results for 
Search instead for 
Did you mean: 

what are the values of following frequencies in STM32F4 discovery example projects?

its
Associate II
Posted on November 28, 2012 at 06:55

RCC_MCO1source_PLLCLK=?

RCC_MCO2source_PLLCLK=?

RCC_MCO2Source_PLLI2SCLK=?

RCC_MCO1Source_LSE=?

and m right for

RCC_MCO1Source_HSI=16 MHz

RCC_MCO2Source_HSE=RCC_MCO1Source_HSE=8MHz

RCC_MCO1Source_SYSCLK=168 MHz

thanks

#mco1 #mco2 #clock
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Posted on November 28, 2012 at 13:08

Well the clocks will need to be enabled, ready, and have crystals present

LSE won't work at all unless you have an external crystal

PLL will be 168 MHz, the fastest you can physically output is 100 MHz, so PLL/2 is 84 MHz

PLLI2S is set to 38.4 MHz

As previously suggested review STM32F4-Discovery_FW_V1.1.0\Project\Demonstration\system_stm32f4xx.c, and measure the pins if this is important.
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..