cancel
Showing results for 
Search instead for 
Did you mean: 

What are the modfication need to do USB work in 180 MHZ?

paramasivan
Associate II
Posted on April 23, 2015 at 14:45

Hi,

      I am using STM32f429 USBH sample codes for one of my project. I have configured USB in FS mode.I have connected a USB keyboard and it works fine in systemcore clock 168 MHZ. When i switched to 180MHZ it stops working. I know, its already mentioned in the header file. what i need to do modify in the code ,USB will work in 180 MHZ?

#!stm32f4-disco
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Posted on April 23, 2015 at 18:57

There isn't a way to provide 48 MHz internally (PLL Q tap) from 180/360 MHz

You'd need to use an external USB PHY.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..