cancel
Showing results for 
Search instead for 
Did you mean: 

Weird Boot up

niklascooke1
Associate II
Posted on October 07, 2009 at 07:24

Weird Boot up

2 REPLIES 2
niklascooke1
Associate II
Posted on May 17, 2011 at 13:25

Hi everybody!

I've got a wierd problem with my board.

Im using Crossworks 1.7, and the problem is that the first time i upload the program to flash it works properly but when the second time i try to upload i get the message ''Loader is not a libmem RPC loader''. when i upload again it works to upload but the program doesnt work properly. The timers and adc wont start up.

The thing i can do to make it work again is to unplug the power supply and upload again. but the second time i upload its the same thing all over again.

I hope you can help me.

Regards Niklas Cooke

danish
Associate II
Posted on May 17, 2011 at 13:25

Have you asked Rowley (the makers of Crossworks)?

In my experience they are helpful and come back with solutions to problems reasonably quickly.

I have had problems with debugging / subsequent downloads when enabling copy-protection or using the debug pins for GPIO. But that should not come as a surprise.

Hope this helps,

Danish