Question
We have SRAM FSMC configuration code available for STM322xG in cubeF2, I want to implement Muxed NOR with the help of same code
Posted on April 15, 2017 at 13:55
Hi,
As the title I want to implement Muxed NOR on STM32F207ZG Nucleo board
following is SRAM read write code.
for (uwIndex = 0; uwIndex < BUFFER_SIZE; uwIndex++) { *(__IO uint16_t*) (SRAM_BANK_ADDR + WRITE_READ_ADDR + 2*uwIndex) = aTxBuffer[uwIndex]; } /* Read back data from the SRAM memory */ for (uwIndex = 0; uwIndex < BUFFER_SIZE; uwIndex++) { aRxBuffer[uwIndex] = *(__IO uint16_t*) (SRAM_BANK_ADDR + WRITE_READ_ADDR + 2*uwIndex); }so for muxed NOR how we will be defining the address and data as it has common address and data lines?
where the control signals are being set?