cancel
Showing results for 
Search instead for 
Did you mean: 

Watchdog timer issue

mskumar_mtech
Associate II

Hello Folks

I have enabled the watchdog timer for 1.5 second. Here is screenshot of watchdog timer configuration for our ready reference.

**

* @brief IWDG Initialization Function

* @param None

* @retval None

*/

static void MX_IWDG_Init(void)

{

 

/* USER CODE BEGIN IWDG_Init 0 */

 

/* USER CODE END IWDG_Init 0 */

 

/* USER CODE BEGIN IWDG_Init 1 */

 

/* USER CODE END IWDG_Init 1 */

hiwdg.Instance = IWDG;

hiwdg.Init.Prescaler = IWDG_PRESCALER_16;

hiwdg.Init.Window = 4095;

hiwdg.Init.Reload = 3000;

if (HAL_IWDG_Init(&hiwdg) != HAL_OK)

{

Error_Handler();

}

/* USER CODE BEGIN IWDG_Init 2 */

 

/* USER CODE END IWDG_Init 2 */

 

}

 

Also I'm clearing the watchdog every 500mSec using the following definition and command.

IWDG_HandleTypeDef hiwdg;

 

HAL_IWDG_Refresh(&hiwdg);

 

Watchdog is not getting cleared and software is resetting at every 1.5 seconds.

 

Am I missing anything here please?

 

Please help me out and respond at the earliest.

 

Many thanks

 

With kind regards

Siva

 

 

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0