2012-05-31 1:05 AM
Hi all,
I have to be sure before I will make another step in my project: Can I wake up the STM32L152 from the STOP mode by any edge on any pin? In other words: can I configure any pin as input to wake up from STOP mode?2012-05-31 11:06 AM
According to the reference manual, you can use any EXTI line, if you enable the corresponding interrupt.
There is a difference if you enter with WFI or WFE - see the respective pages 75 + 184 of the ref. manual.2012-06-01 3:02 AM
Yes, I saw the manual.
I made test on different pins and only those with additional WKUP function worked properly.