2018-03-15 12:06 AM
Hi,
I am using a STM32LO72 device and entering stop mode using
HAL_PRW_EnterSTOPMode ( PWR_LOWPOWERREGULATOR_ON, PWR_STOPENTRY_WFI);
I have configured the RTC AlarmB to wake the device but it wakes almost inmmediately.
Would anyone have advice on how to tell which interrupt has caused the exit from STOP mode?
Thank You
Regards
#stop-mode-wake-source2018-03-15 12:30 AM
Things I've done to track this down: First check EXTI to see which interrupts are enabled. Take a look at RTC->ISR for any other active RTC sources. Set a breakpoint just before the WFI to see if any EXTIs are pending.
Pending EXTIs are going to clear right after the WFI so you need to catch anything that's active before entering STOP. The EXTI mask register will tell you the possible sources to narrow it down.
I don;t use the HAL so no idea what it enables.
Jack Peacock
2018-03-15 2:17 AM
,
,
Hi Jack,
Thank you very much for your replay
I have written 0x00000000 to the EXTI_IMR register and that device does not wake
I have written 0x00020000 to the EXTI_IMR register and that device does wake nearly immediately so the interrupt is coming from the RTC on line 17
I have the EXTI line 17 set up as MODE_IT and TRIGGER_RISING
I broke before entering power mode at the RTS->, ISR has the following set
RSF
WUTWF
ALRBWF
ALRAWF
Thank you
Regards
Peter Simpson
<,https://community.st.com/?et=watches.email.thread>, STMicroelectronics Community
Re: Wake from stop mode
reply from Jack Peacock <,https://community.st.com/0D70X000006Sjg7SAC
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.