2017-05-02 1:54 AM
I am using a STM32L476VG (100 pin package, VREF+ not bonded to VDDA) for a mixed signal design. I planed to use the VREF+ as a 2.048V reference output. Currently there is no load on the VREF+ pin.
Unfortunately I always get a HAL_TIMEOUT while waiting for the VRR bit in the VREFBUF CSR register:
HAL_SYSCFG_VREFBUF_VoltageScalingConfig(SYSCFG_VREFBUF_VOLTAGE_SCALE0);
HAL_SYSCFG_VREFBUF_HighImpedanceConfig(SYSCFG_VREFBUF_HIGH_IMPEDANCE_DISABLE);
if (HAL_SYSCFG_EnableVREFBUF() != HAL_OK)
{
Error_Handler(ENVREFO_ERROR);
}�?�?�?�?�?�?Also no voltage output is measureable at the VREF+ pin...
Do I miss something here? I tried to change the order or manually set the registers (without time-out) but no output at all.
Thank you for your help!!
Best regards,
Merlin
#analog #vrefbuf #reference #vref+ #csrSolved! Go to Solution.
2017-05-04 1:40 AM
For everyone having the same problem:
Enable clock for SYSCFG: Set bit 0 in RCC_APB2ENR before enabling the VREFBuffer.
2017-05-04 1:40 AM
For everyone having the same problem:
Enable clock for SYSCFG: Set bit 0 in RCC_APB2ENR before enabling the VREFBuffer.