2014-01-31 12:34 PM
Hello
I want to make a voltmeter using my STM32F4 discovery , actually these are my first steps and I am facing some problems and I need some help.Thank you very much. #lmgtfy2014-02-11 7:44 AM
Jumper the VDD and BOOT0 pins, restart the board, attach via ST-LINK Utilities, Connect and Erase part.
http://www.st.com/web/en/catalog/tools/PF258168
2014-02-11 8:33 AM
Thank you very much clive1 , it works!
the problem is solved .2014-02-11 12:28 PM
2014-02-11 12:42 PM
http://www.lmgtfy.com?q=current+sensor
2014-02-12 1:56 AM
''
'' Now that is just mean and UNHELPFUL. ''I want to make an Ammeter using my stm32f4 , any ideas please. (I prefer not to use the shunt)'' A shunt is easier and not that bad - most multimeters use the shunt meathod. OK - what is a shunt - just a resistor! The Shunt resistor is placed 'in line' with the power source. So all the current to the circuit flows through the shunt resistor. Volt = Amp X Ohm therefore Amps = Volts / Ohms If you use a 1Ohm shunt resistor - the current is simply the Volts measured across the shunt resistor. If you do NOT want to use a shunt - then look at the current clamp devices (it is just a special, calibrated Hall effect sensor in a ferrite core) that are available. They will have data sheets.2014-02-12 2:29 AM
''
http://www.lmgtfy.com/?q=current+sensor
''Now that is just mean and UNHELPFUL.
I don't think so.If someone likes to deal with such complex matters as Cortex-M MCUs, and carries 'student' as part of his nickname, it's only fair to expect a certain amount of individual initiative.If the OP neither knows any concept of measuring electrical currents, nor is able to look up such things himself, he'd better return to some more basic projects.
2014-02-12 8:20 AM
Thank you for your response.
2014-02-12 8:24 AM
Thank you for your response.
2014-02-12 10:36 AM
No offense intended.
Neil's posts are often quite outspoken, but nonetheless true.2014-02-12 11:03 AM
I prefer not to use the shunt''
Why?What specific objection(s) do you have to using a shunt?If you don't state the reason(s), how can people avoid making suggestions which might suffer from the same - or worse - problems...?!We’re moving the ST Community to a new platform to give you a better and more reliable community experience.