cancel
Showing results for 
Search instead for 
Did you mean: 

Virtual COM port driver 1.4.0 doesn't work with CDC examples

peterdonchev
Associate III
Posted on February 02, 2015 at 21:22

Hi, I have a problem with virtual com port driver 1.4.0. CDC devices are not recognized, when this driver is installed, but I don't have problem with the old driver (1.3.1) under Windows 7. I must be sure that CDC device will work under Windows 8.1. Where is the problem?

10 REPLIES 10
slimen
Senior
Posted on October 11, 2016 at 12:29

Hello,

You can follow ''CDC-Standalone'' example in STM32cubeF0, it may be helpful:

STM32Cube_FW_F0_V1.6.0\Projects\STM32072B_EVAL\Applications\USB_Device\CDC_Standalone

But, there is no working example with Coocox IDE.

PS: Please, avoid mixing new discussion in the old thread, and creating a new one for your issue, this will be more easy for user forum.

Regards