2009-08-16 2:55 AM
Very basic PWM output pin question
2011-05-17 4:20 AM
Folks, I'm just laying out my first STM32 board and I want to be absolutely sure I understand the PWM output pin assignment correctly.
I'm using an F101 in the 36 pin package. Do I understand correctly that the TIMx_CHy pins can all be assigned as PWM outputs where x = timer number and y=channel number? I am reasonably sure that's the case, but as it's the QFN package and I have absolutely no chance to mod it if wrong, I really want to be certain! Many thanks, Rob2011-05-17 4:20 AM
Good 'ere, innit?