2012-06-01 03:17 AM
Can anyone post a link to a working Virtual COM port example for the STM32F4 discovery board.
-gandalf #vcp-download-drivers2012-06-02 10:09 AM
Gandalf,
See my project : New Project Download - Virtual Com with Cmd Shell and ADC Reading Page - see Virtual Com Project for Descriptrion and Download : [[this link/image has been flagged as malicious by our security scan software and has been deleted]]2012-06-04 02:34 AM
Thanks for the quick reply jlc.jlsilicon. I code is running fine. Could you please provide me with a link to the serial.inf driver, i am using windows xp SP3. If would really appreciate it if you could give me a link from where i can download the driver.
-Gandalf2012-06-04 11:26 AM
jlsilicon,
Ive installed the VCP driver that STmicro provides in its website. With the code running on the board when connected to the PC, XP asks me to install a driver for the USB device. Which driver do i install ? I little help would be appreciated. -gandalf2012-06-05 01:40 AM
Okay Gandalf,
Let me see if I can find it, or modify the code with an alternate.2012-07-24 12:14 PM
Hello,
I also have a problem with finding working virtual COM port drivers for this project. Anyone could provide a link, please? I am running Windows 7 64-bit. Thanks, Kelnerrr2012-07-24 12:42 PM
Page - see Virtual Com Project for Descriptrion and Download :
Wikisend links are broken.
https://my.st.com/public/STe2ecommunities/mcu/Lists/STM32Discovery/Flat.aspx?RootFolder=https://my.st.com/public/STe2ecommunities/mcu/Lists/STM32Discovery/New Project Download - Virtual Com with Cmd Shell and ADC Reading&FolderCTID=0x01200200770978C69A1141439FE559EB459D75800084C20D8867EAD444A5987D47BE638E0F¤tviews=318
2012-07-24 01:08 PM
Hi Clive,
I've searched the project page for any info where to grab the working driver for vcp. No luck. Would you mind sending it to kelnerrr at gmail.com? Thanks, Kelnerrr2012-07-24 03:48 PM
I've emailed you, but for general consumption these are the most recent VCP drivers I'm aware of.
http://dekar.wc3edit.net/st website/VCP_Setup.zip
http://www.st.com/internet/com/SOFTWARE_RESOURCES/SW_COMPONENT/SW_DRIVER/stm32_vcp.zip
https://my.st.com/public/STe2ecommunities/mcu/Lists/STM32Discovery/Flat.aspx?RootFolder=https://my.st.com/public/STe2ecommunities/mcu/Lists/STM32Discovery/New Project Download - Virtual Com with Cmd Shell and ADC Reading&FolderCTID=0x01200200770978C69A1141439FE559EB459D75800084C20D8867EAD444A5987D47BE638E0F¤tviews=318
2012-07-25 02:33 PM
Going to confirm from my own testing that the last link, which contains the v1.3.1 drivers for x64 works in Win 7 against a VCP/CDC example built from the USB FW library which I have ported.
STM32_USB-Host-Device_Lib_V2.1.0\Project\USB_Device_Examples\VCPhttps://my.st.com/public/STe2ecommunities/mcu/Lists/STM32Discovery/Flat.aspx?RootFolder=https://my.st.com/public/STe2ecommunities/mcu/Lists/STM32Discovery/New Project Download - Virtual Com with Cmd Shell and ADC Reading&FolderCTID=0x01200200770978C69A1141439FE559EB459D75800084C20D8867EAD444A5987D47BE638E0F¤tviews=318