Using USB Hid to send float/double
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2011-05-29 1:53 PM
Hi,
I just started working with Hid class to communicate via USB with STM32F103VB. I managed to send few bytes of data at once using
UserToPMABufferCopy(Send_Buffer, ENDP1_TXADDR, 5);
where Send_Buffer is declared as
u8 Send_Buffer2[5];
It works fine but is there a simple way to send floats or double variables in a simple way or do I have to make a conversion from seperate bytes to a variable I want to send? I'm real beginner so sorry if this is a silly qustion :)
Thanks in advance.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2011-05-29 6:25 PM
Probably like this would suffice :
double AssortedMeasurements[12]; UserToPMABufferCopy((void *)AssortedMeasurements, ENDP1_TXADDR, sizeof(AssortedMeasurements) ); That or use some generic struct or union.Up vote any posts that you find helpful, it shows what's working..
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2011-05-30 3:42 PM
Unfortunately that didn't work.. It's impossible to read any data from the device. Any other hints?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2011-05-31 9:51 AM
Unfortunately that didn't work.. It's impossible to read any data from the device. Any other hints?
Didn't work? The device didn't send it, or you couldn't do anything with it at the receiving end? You couldn't read any data, or decipher it? Please be more specific, and provide example data. As you're trying to send binary data, you'll have to reconstitute it on the correct boundaries at the destination. Want it as ASCII, use sprintf(), and send the resultant data.Up vote any posts that you find helpful, it shows what's working..
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2011-06-01 2:44 AM
On the host side I am using ReadFile function to obtain the report but it timeouts and reads no data. So I decided to take a step backwards and try to send an integer the same way you proposed. This time I was able to read data form the device. The code looks like this:
int AssortedMeasurements[2];
AssortedMeasurements[0]=5;
AssortedMeasurements[1]=280;
UserToPMABufferCopy((void *)AssortedMeasurements, ENDP1_TXADDR, sizeof(AssortedMeasurements) );
I've set my report descriptor like this:
const u8 CustomHID_ReportDescriptor[CUSTOMHID_SIZ_REPORT_DESC] =
{
0x05, 0x8c, // USAGE_PAGE (ST Page)
0x09, 0x01, // USAGE (Demo Kit)
0xa1, 0x01, // COLLECTION (Application)
// 6
// ------ common globals ------
0x15, 0x00, // LOGICAL_MINIMUM (0)
0x26, 0x2c, 0x01, // LOGICAL_MAXIMUM (300)
0x75, 32, // REPORT_SIZE (32) bits
// ------ input report ------
0x85, 0x05, // REPORT_ID (5)
0x95, 1,
// REPORT_COUNT
0x09, 0x01, // USAGE (Vendor Usage 1)
0x81, 0x02, // INPUT (Data,Var,Abs)
// ------ output report ------
0x85, 0x03, // REPORT_ID (3)
0x95, 1,
// REPORT_COUNT
0x09, 0x01, // USAGE (Vendor Usage 1)
0x91, 0x02, // OUTPUT (Data,Var,Abs)
// ------ output report 2 ------
0x85, 0x04, // REPORT_ID (3)
0x95, 1,
// REPORT_COUNT
0x09, 0x02, // USAGE (Vendor Usage 1)
0x91, 0x02, // OUTPUT (Data,Var,Abs)
0xc0 // END_COLLECTION
};
The problem is that my integer value is being send as one byte. So if I try to send more than 255 it just wraps around itself (f.e. 280 turns to 280-256=24). I am looking for a way to send my integer value as one number, I was hoping that REPORT_SIZE(32) would do the trick but unfortunately it didn't. Any clues please?
EDIT: I've managed to send float using an union. I just had to find out what an union is first. Still, if anyone has a better solution it would be greatly appreciated. Thanks anyways for your help!