2020-07-27 5:55 AM
Hi, I'm using Nucleo-L432KC board and I've got quite a few devices plugged in to it already. And I need to add another device using UART, but I'm using UART2 for debug output already and I2C1 (which always shares pins with UART1) for a couple i2C devices.
So my question is - Is it ok to put UART device with I2C devices on the same line (bus)? If I communicate with my I2C devices infrequently enough could occasional UART transmission on the same line make them malfunction? Or maybe that's complete lunacy...
Thank you for any suggestions.
2020-07-27 8:16 AM
you can use sda line for whatever you want as long as scl is low. that's safe. find another pin.
2020-07-27 10:47 AM
Seems like a bad plan, I2C device likely to get confused, have pattern sensitivity