cancel
Showing results for 
Search instead for 
Did you mean: 

Using STM32 to synchronize a multiple output power supply

Omri G
Associate
Posted on December 06, 2016 at 09:49

Hi all, 

I want to start using STM32 MCU in order to synchronize a multiple output power supply with a single frequency.

So for I have used an anlog PLL (74HC4046) for this purpose:

1. The relevant range is 200-500 Khz.

2. If the external freq. is out of range or doesn't exist the internal 400Khz clock will distribute to all module. 

First of all, is it possible? 

and if so, are there any examples?

I am using STM32L053 Discovery.

Thanks.

#power-supply #stm-32 #stm32-discovery
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Imen.D
ST Employee
Posted on December 07, 2016 at 10:36

Dear

g.omri

,

Welcome to STM32 community

The STM32CubeL0 firmware package comes with a rich set of examples as described in

http://www.st.com/content/ccc/resource/technical/document/application_note/c4/d9/35/24/7f/10/49/fc/DM002097pdf/files/DM002097pdf/jcr:content/translations/en.DM002097pdf

and there is several PWR examples at this path: STM32Cube_FW_L0_V1.8.0\Projects\STM32L053C8-Discovery\Examples\PWR

You can refer to the manual

http://www.st.com/content/ccc/resource/technical/document/reference_manual/2f/b9/c6/34/28/29/42/d2/DM000957pdf/files/DM000957pdf/jcr:content/translations/en.DM000957pdf

,is your reference for more clarification.

Best Regards

-Imen-

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen