2013-03-30 11:25 AM
Hi
I would like to apply an automatic system reset in case a particular condition in my system is met. I already know how to apply a system reset through software. Now I want also to do it via hardware. If If I pull pin NRST high, will it have the same effect as when I press push button B2?Thanks,Terence2013-03-30 02:05 PM
No, you'd want a pull up to hold in the normally high state, and then drive it LOW using an OD driver to reset it. You should not drive this pin high with a PP driver.
2013-03-31 02:14 PM
Thanks for your reply; but can you please explain more clearly, as I cannot understand the terms OD and PP driver.
Thanks in advance Terence2013-03-31 05:49 PM
OD - Open Drain
http://en.wikipedia.org/wiki/Open_collector
PP - Push-Pullhttp://en.wikipedia.org/wiki/Push%E2%80%93pull_output
http://digital.ni.com/public.nsf/allkb/D9B4018C3E540CE4862570F30068C0DB