2019-02-12 2:46 AM
Hi community,
I'm currently trying to set/reset the BFB2 bit from application program, under MBed, with a STM32L476RG.
Though setting/reseting BFB2 can be done properly thru ST-LINK, I did not manage in modifying the option bytes, using the HAL/LL drivers.
The code I've tried looks like:
void OptionByteSet(bool bfb2)
{
int retCode;
FLASH_OBProgramInitTypeDef optionBytes; // Structure that holds the option bytes to be programmed
printf("\r\n*********************** SETTING BFB2 ****************************");
if(HAL_FLASH_Unlock()==HAL_OK) // Unlock the flash controls registers
printf("\r\n\tHAL_FLASH_Unlock -> OK");
else
printf("\r\n\tHAL_FLASH_Unlock -> Failure");
if (HAL_FLASH_OB_Unlock()==HAL_OK) // Unlock the option bytes controls registers
printf("\r\n\tHAL_FLASH_OB_Unlock -> OK");
else
printf("\r\n\tHAL_FLASH_OB_Unlock -> Failure");
HAL_FLASHEx_OBGetConfig(&optionBytes); // Get current optionbytes configuration
printf("\r\n-------------------Before modifications");
OptionByteDisplay(&optionBytes);
optionBytes.OptionType = OPTIONBYTE_USER;
optionBytes.USERType = OB_USER_BFB2;
if (bfb2) // Set the bfb2 option bit as needed
optionBytes.USERConfig |= OB_BFB2_ENABLE;
else
optionBytes.USERConfig &= ~OB_BFB2_ENABLE;
printf("\r\n-------------------Projected modifications");
OptionByteDisplay(&optionBytes);
if ((retCode=HAL_FLASHEx_OBProgram(&optionBytes))==HAL_OK)
printf("\r\n\r\n BFB2 Configuration OK");
else
printf("\r\n\r\n BFB2 Configuration Failure, code=%02X",retCode);
HAL_FLASH_OB_Lock();
HAL_FLASH_Lock();
retCode = HAL_FLASH_OB_Launch();
printf("\r\n\r\n BFB2 Validation, code=%02X",retCode);
printf("\r\n-------------------After modifications");
HAL_FLASHEx_OBGetConfig(&optionBytes); // Get current optionbytes configuration
OptionByteDisplay(&optionBytes);
}The output I get is the following:
*********************** SETTING BFB2 ****************************
HAL_FLASH_Unlock -> OK
HAL_FLASH_OB_Unlock -> OK
-------------------Before modifications
OPTION BYTES
OptionType = 00000007
WRPArea = 00000000
WRPStartOffset = 000000FF
WRPEndOffset = 00000000
RDPLevel = 000000AA
USERType = 20000014
USERConfig = FFAFF800
PCROPConfig = 5C613118
PCROPStartAddr = 00000000
PCROPEndAddr = 00000000
-------------------Projected modifications
OPTION BYTES
OptionType = 00000004
WRPArea = 00000000
WRPStartOffset = 000000FF
WRPEndOffset = 00000000
RDPLevel = 000000AA
USERType = 00000080
USERConfig = FFBFF800
PCROPConfig = 5C613118
PCROPStartAddr = 00000000
PCROPEndAddr = 00000000
BFB2 Configuration Failure, code=01
BFB2 Validation, code=00
-------------------After modifications
OPTION BYTES
OptionType = 00000007
WRPArea = 00000000
WRPStartOffset = 000000FF
WRPEndOffset = 00000000
RDPLevel = 000000AA
USERType = 00000080
USERConfig = FFAFF800
PCROPConfig = 5C613118
PCROPStartAddr = 00000000
PCROPEndAddr = 00000000
What am I missing there ? I'm stuck at this point, and cannot either point out why nor think about anything else to try, since two weeks now.
2019-10-10 5:53 AM
Hello,
I've had some problem to modify the BFB2 bit using examples found on the internet.
Finally, I managed to get it to work by clearing the FlashOB_ProgramInitTypedef structure in order to make sure only the BFB2 bit will be written.
Below is the working code which makes a toggle of the BFB2 :
FLASH_OBProgramInitTypeDef optionBytes;
uint8_t setOrReset;
__disable_irq();
HAL_FLASH_Unlock();
HAL_FLASH_OB_Unlock();
HAL_FLASHEx_OBGetConfig(&optionBytes); // Get current optionbytes configuration
// If BFB2 set, we will reset it
if ( optionBytes.USERConfig & OB_BFB2_ENABLE ){
setOrReset = 0;
}else{
setOrReset = 1;
}
// Clean structure before using it for option bytes writing :
memset((void*)&optionBytes,0,sizeof(optionBytes));
optionBytes.OptionType = OPTIONBYTE_USER;
optionBytes.USERType = OB_USER_BFB2;
if (setOrReset // Set the bfb2 option bit as needed
optionBytes.USERConfig = OB_BFB2_ENABLE;
else
optionBytes.USERConfig = OB_BFB2_DISABLE;
if (HAL_FLASHEx_OBProgram(&optionBytes)==HAL_OK)
{
HAL_FLASH_OB_Launch();
}
HAL_FLASH_OB_Lock();
HAL_FLASH_Lock();
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.