Visitor II
September 10, 2013
Question
Use of multiple analog functions of same pin possible?
- September 10, 2013
- 1 reply
- 730 views
Posted on September 10, 2013 at 15:32
Hello guys!
I wonder if it is possible to use more than one additional function if the pin is configured as an analog input. I can not find any detail in the datasheet or reference manual that denies or allows this kind of usage especially. For instance (see attachment): Is it possible to use PA1 as input for COMP1 and OPAMP1 on the STM32F302RC at the same time?https://my.st.com//public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Attachments/33802/Multipin.png
Thanks for your help. Greetings, Benny #multiple-pin #multiply-functions