cancel
Showing results for 
Search instead for 
Did you mean: 

SWD Hardware question

jksystem247
Associate II
Posted on October 10, 2013 at 05:18

Hi, I am new to the STM32 MCU.

I am confused as to how to do In-circuit Serial programming with STM32F0 processors.

F0 line doesn't seem to have JTAG option, but it has SWD option.

So, For SWD, how should the DATA,CLK,/RST line for the ICSP look like?

can i just directly connect the two without any pull-up/down resistors?

In other words, if I make the connection as below, would my development environmen recognize the STM32F0 MCU via STLINK/V2 and be able to both program and debug it?

STM32           STLINK/V2

GND     <===>   GND

VDD      <===>   VDD

SWDIO  <===>    SWDIO(JTAG TMS)

SWCLK <===>    SWCLK(JTAG TCK)

/RST     <===>    /RST

Thank you.

#stm32-swd
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
jzawadzk
Associate II
Posted on October 10, 2013 at 20:39

I can confirm that this works for F1 series. I guess that there is no reason why this wouldn't work for F0.