cancel
Showing results for 
Search instead for 
Did you mean: 

USB Virtual Com port missing bytes periodcially

alexpabouct9
Associate II
Posted on March 19, 2011 at 13:52

USB Virtual Com port missing bytes periodcially

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
saimaddy123
Associate II
Posted on May 17, 2011 at 14:28

I could have the stdio routed through VCOM. I did not see any issue like you mentioned. I made it work for STM32F107VCT6. However, you can replace USB_Sil_Write/USB_Sil_Read with corresponding Set_EPTX_XXX APIs in order to have it working...Here is the link

[DEAD LINK /public/STe2ecommunities/mcu/Lists/ARM%20CortexM3%20STM32/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/ARM CortexM3 STM32/stdio over USB serial in STM32-H107&FolderCTID=0x01200200770978C69A1141439FE559EB459D758000626BE2B829C32145B9EB5739142DC17E&TopicsView=https://my.st.com/public/STe2ecommunities/mcu/Lists/ARM%2520CortexM3%2520STM32/AllItems.aspx&currentviews=97]https://my.st.com/public/STe2ecommunities/mcu/Lists/ARM%20CortexM3%20STM32/Flat.aspx?RootFolder=%2fpublic%2fSTe2ecommunities%2fmcu%2fLists%2fARM%20CortexM3%20STM32%2fstdio%20over%20USB%20serial%20in%20STM32-H107&FolderCTID=0x01200200770978C69A1141439FE559EB459D758000626BE2B829C32145B9EB5739142DC17E&TopicsView=https%3A%2F%2Fmy%2Est%2Ecom%2Fpublic%2FSTe2ecommunities%2Fmcu%2FLists%2FARM%2520CortexM3%2520STM32%2FAllItems%2Easpx&currentviews=97