2021-09-08 5:28 PM
Hello,
I experienced a phenomenon in which the USB port was not reconnected.
This phenomenon occurs when a USB port is connected to the product and reboots.
I check my device manager.
When i turn off product, com port also disappear.
and product reboot then com port appear.
But i can't receive any data.
When i reconnect USB cable then communication work well.
Summary
I need your support.
Thanks. best regards.
Solved! Go to Solution.
2021-09-08 6:59 PM
I solved this problem.
It need USB gpio pull down.
If device restart then USB gpio pull down.
2021-09-08 6:29 PM
After the device restarts, do you see the enumeration process? If not, it's the time to unpack your USB bus analyzer,
2021-09-08 6:59 PM
I solved this problem.
It need USB gpio pull down.
If device restart then USB gpio pull down.
2021-09-08 7:02 PM
Huh? What is a USB gpio pull down?
2021-09-09 7:22 PM
USB_OTG_FS_DM, USB_OTG_FS_DP need pull down.