cancel
Showing results for 
Search instead for 
Did you mean: 

USB PD (UCPD) on STM32H562

AWack
Associate III

Hi,

I´ve problems getting UCPD running on a STM32H563. With STM32G0 I´ve alraedy realized a lot of such projects with UCPD. Hence I suggest, that it maybe is a problem of the DMA which is much more complicated to configure on the H5. Is there any information about how to configure UCPD on H5?

Best,

Achim

3 REPLIES 3
FBL
ST Employee

Hi @AWack 

Here you can find example firmware of UCPD on H563. If still having issues linked to UCPD and DMA configuration, provide more details to help you further.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.


AWack
Associate III

Hi FBL,

unfortunately I still don´t get 20V. Also checked the measured USB voltage in usbpd_pwr_user.c

Please find attached a USB PD log. it infinitely request the source capabilities...

 

FBL
ST Employee

Hi @AWack 

EPR should be supported using our stack. However, as of now we don't have an example firmware to reach 20V and hardware setup to test this. Based on your screenshot, it seems EPR mode, is still not configured! 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.