2010-04-27 2:12 AM
USB Lib and Standby, problem on Wakeup
2011-05-17 4:48 AM
Mine does not wake up from Standby.
I currently do it like this: ...// Peripheral Clock - This is done in the init function, but I did it again here
RCC_APB1PeriphClockCmd(RCC_APB1Periph_PWR,ENABLE); // Enable WKUP pin PWR_WakeUpPinCmd(ENABLE);// Insert a delay - I have also tried without this delay
Delay(0xFFFF); // for(; nCount != 0; nCount--);// Request to enter STANDBY mode and wake up with rising edge of WKUP pin
PWR_EnterSTANDBYMode();while(1)
{ // Infinite loop - It's OK because the system will reset anyways } The unit does not wake up (reset). I've tried with both the JTAG connected and not connected. Port PA.0 (WKUP pin) has a pull-down resistor, leading to a momentary switch, with Vcc on the other side of the switch, which should be enought to generate the required rising edge when the button is pressed. Any ideas? Thanks!