Skip to main content
tuyenvquang
Associate
April 14, 2015
Question

USB DISCONNECT/CONNECT in STM32F107

  • April 14, 2015
  • 0 replies
  • 481 views
Posted on April 14, 2015 at 04:51

I am developing a HID USB with STM32F107, and iam currently using STM32_USB-FS-Device_Lib_V4.0.0. 

1. My problem is that i dont understand clearly about USB_DISCONNECT feature in this MCU.

2. I see in the library, ST define some GPIO for USB disconnect

#if defined(STM32L1XX_MD) || defined(STM32L1XX_HD)|| defined(STM32L1XX_MD_PLUS)|| defined(STM32F37X)|| defined(STM32F30X)

  /* Enable the SYSCFG module clock (used for the USB disconnect feature) */

  RCC_APB2PeriphClockCmd(RCC_APB2Periph_SYSCFG, ENABLE);

and 

/* Define the STM32F10x hardware depending on the used evaluation board */

#ifdef USE_STM3210B_EVAL

  #define USB_DISCONNECT                      GPIOD  

  #define USB_DISCONNECT_PIN                  GPIO_Pin_9

  

  #define RCC_APB2Periph_GPIO_DISCONNECT      RCC_APB2Periph_GPIOD

  #define RCC_APB2Periph_ALLGPIO              (RCC_APB2Periph_GPIOA \

                                               | RCC_APB2Periph_GPIOB \

                                               | RCC_APB2Periph_GPIOC \

                                               | RCC_APB2Periph_GPIOD \

                                               | RCC_APB2Periph_GPIOE )

It seems that different boards have different pin configuration for USB disconnect.

So, how can i know which GPIO pin is USB Disconnect in my MCU.

3. Difference between internal USB pullup vs external USB pullup
    This topic has been closed for replies.