cancel
Showing results for 
Search instead for 
Did you mean: 

USB Disconnect circuit

joe23
Associate II
Posted on August 19, 2014 at 13:45

0690X00000602wLQAQ.jpg

I've been looking through STM32 development board circuits to find the best way to connect the USB disconnect. I found the above circuit from the STM3210E-EVAL board, but all of the ST boards appear to have similar layouts. I have a couple questions about this layout:

  1. Why are there two transistors? Why isn't T2 sufficient?
  2. Why are there transistors at all? Could USB_DP be connected to a GPIO via a resistor and toggle between floating and on?
  3. If not 2, could a P-CH MOSFET with a low VGS be used instead?
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0