cancel
Showing results for 
Search instead for 
Did you mean: 

USB Device won't enumerate on custom F7 board

Mike Hooper
Senior
Posted on December 05, 2017 at 15:34

I have a custom F7 board configured as a USB HID device (using CubeMX generated code) that won't enumerate with my PC host. However, if I pull BOOT0 high, it will enumerate as a 'STM Device in DFU Mode'. So I assume my hardware is working properly.

I have stepped through the initialization code and everything seems to be getting properly initialized (all functions return USBD_OK). However, there is no activity on the D+/D- lines as if they are not getting powered up.

Can anyone give some guidance on this?

Thanks,

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0