cancel
Showing results for 
Search instead for 
Did you mean: 

USB-C audio port and charging

VIJAY212
Associate

HI 

USB-C Input (5–20 V PD) + USB-C Data (USB2.0 D+/D– to STM32H745) + charging phone at same time + Audio data transfer

Problem: 

When I connect the USB-C input supply (PD 5–20 V), the phone only charges and the audio USB port does NOT appear.
But when I do NOT provide PD input power, the audio USB port appears correctly.
And if the audio port is already active, then when I connect the PD input afterwards, the phone does NOT charge — only the audio stays active 

VIJAY212_1-1763640168685.png

 

VIJAY212_0-1763640112560.png

 

1 REPLY 1
FBL
ST Employee

Hi @VIJAY212 

First, schematics in the screenshot are not clear!

Second, STM32H745 doesn't embed UCPD controller to manage power delivery. You need external PD IC or different MCU supporting UCPD controller to handle power delivery and transfer data.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.




Best regards,
FBL