cancel
Showing results for 
Search instead for 
Did you mean: 

usart1 and usart2 contention

dvcosta43
Associate II
Posted on July 15, 2014 at 17:19

Hello again.

I've two usarts in use on my board. One, Usart1 is connected to the console and the other usart2 is connected to a modem chip. When I enable the usart2 interrupt using the NVIC commands, there is no output to the console from usart1 and when I comment the usart2 NVIC commands, output to the console is normal but then usart2 interrupt handling is disabled. I need both working simultaneously. It looks as if there is some sort of priority contention.

Both usarts are fine individually as their handlers are being activated.

Any help greatly appreciated.

Dave

    void Usart1Init(void)

    {

USART_InitTypeDef USART_InitStructure;

GPIO_InitTypeDef GPIO_InitStructure;

NVIC_InitTypeDef NVIC_InitStructure;        

        

//NVIC_InitTypeDef NVIC_InitStructure;      

        

    RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOA , ENABLE);    

    RCC_APB2PeriphClockCmd(RCC_APB2Periph_USART1, ENABLE);

//  RCC_APB2PeriphClockCmd( RCC_APB2Periph_AFIO, ENABLE);    

  /* Enable the USART1 Interrupt */

  NVIC_InitStructure.NVIC_IRQChannel = USART1_IRQn;    

  NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0;

    NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0;    

  NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;

  NVIC_Init(&NVIC_InitStructure);        

        

  GPIO_InitStructure.GPIO_Pin = GPIO_Pin_9;             

  GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF_PP;

  GPIO_InitStructure.GPIO_Speed = GPIO_Speed_10MHz;

  GPIO_Init(GPIOA, &GPIO_InitStructure);           

  GPIO_InitStructure.GPIO_Pin = GPIO_Pin_10;            

  GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IN_FLOATING;  

  GPIO_InitStructure.GPIO_Speed = GPIO_Speed_10MHz;

  GPIO_Init(GPIOA, &GPIO_InitStructure);

          

        

  USART_InitStructure.USART_BaudRate = 9600;

  USART_InitStructure.USART_WordLength = USART_WordLength_8b;

  USART_InitStructure.USART_StopBits = USART_StopBits_1;

  USART_InitStructure.USART_Parity = USART_Parity_No;

  USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None;

  USART_InitStructure.USART_Mode = USART_Mode_Rx | USART_Mode_Tx;

    

   USART_ITConfig(USART1, USART_IT_TXE, ENABLE);

       

  USART_ITConfig(USART1, USART_IT_RXNE, ENABLE);        

  COMInit(COM1, &USART_InitStructure);       

    }

PUTCHAR_PROTOTYPE

{

    /* Place your implementation of fputc here */

    /* e.g. write a character to the USART */

    

    while(USART_GetFlagStatus(USART1, USART_FLAG_TXE) == RESET); // Wait for Empty

    USART_SendData(USART1,(u8)ch);

    return ch;

}

void Usart2Init(void)

{        

  USART_InitTypeDef USART_InitStructure;

  GPIO_InitTypeDef GPIO_InitStructure;

    NVIC_InitTypeDef NVIC_InitStructure;

 

  // Enable GPIOA clock

  RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOA , ENABLE);

 

  // Enable USART2 APB clock

  RCC_APB1PeriphClockCmd(RCC_APB1Periph_USART2, ENABLE);

    

  // USART2 IRQ Channel configuration

  NVIC_InitStructure.NVIC_IRQChannel = USART2_IRQn;

  NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 1;

    NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0;

  NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;

  NVIC_Init(&NVIC_InitStructure);    

// Doesn't look as if I need these   

//  RCC_APB1PeriphClockCmd(RCC_APB2Periph_AFIO, ENABLE);    

//  GPIO_PinRemapConfig(GPIO_Remap_USART2, ENABLE);

    

   

  GPIO_InitStructure.GPIO_Pin = GPIO_Pin_2;             

  GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF_PP;

  GPIO_InitStructure.GPIO_Speed = GPIO_Speed_10MHz;

  GPIO_Init(GPIOA, &GPIO_InitStructure);           

  GPIO_InitStructure.GPIO_Pin = GPIO_Pin_3;            

  GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IN_FLOATING;  

  GPIO_InitStructure.GPIO_Speed = GPIO_Speed_10MHz;

  GPIO_Init(GPIOA, &GPIO_InitStructure);

  

  USART_InitStructure.USART_BaudRate = 115200;

  USART_InitStructure.USART_WordLength = USART_WordLength_8b;

  USART_InitStructure.USART_StopBits = USART_StopBits_1;

  USART_InitStructure.USART_Parity = USART_Parity_No;

  USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None;

  USART_InitStructure.USART_Mode = USART_Mode_Rx | USART_Mode_Tx;

  USART_Init(USART2, &USART_InitStructure);

    USART_ITConfig(USART2, USART_IT_TXE, ENABLE);

  USART_ITConfig(USART2, USART_IT_RXNE, ENABLE);

    USART_Cmd(USART2, ENABLE);   

    }

void USART2_IRQHandler(void)

{

uint8_t rx_byte = 0;

static int rx_count = 0;

  

            

  if (USART_GetITStatus(USART2, USART_IT_RXNE) != RESET)

  {   

        rx_byte = USART_ReceiveData(USART2);        

    rx_buf[rx_count++] = rx_byte;        

    if (rx_count >= (sizeof(rx_buf) - 1))

      rx_count = 0;

  }               

}
This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
Posted on July 15, 2014 at 17:38

Don't enable TXE interrupts unless you plan on servicing them with data.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
dvcosta43
Associate II
Posted on July 15, 2014 at 18:46

Hello Clive,

Do you mean...unless I am sending data in the USART2_Handler, then I should keep this disabled? I am sending strings to the modem just not through the handler.

Dave

Posted on July 15, 2014 at 19:43

So why enable the interrupt?

Understand that the interrupt will keep re-entering, indefinitely, if the TXE status bit is asserted, and you have the interrupt enabled. If you do not supply it with data, it will never clear, and your foreground code will never get to execute.
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..