2018-11-10 12:53 AM
Hello,
I am a beginner to Nucleo-64 board programming and I am trying to work on USART communication of it. I am using NUCLEO-L476RG board and STM32CubeLL library for configuring USART and starting communication with it.
Programming Scenario:
I have connected Tx and Rx of USART2 together on the board. I want to transmit a string and receive the same string on the corresponding Rx pin. I have used interrupt based reception and I don't want to use DMA for it. I am getting the string on the Rx pin but the receive buffer is getting populated with the characters from aRxBuffer[2] position. Please help me to find the reason behind it.
My code:
void SystemClock_Config(void);
void Configure_GPIO(void);
void SendTo_USART(void);
void Configure_USART(void);
uint8_t aTxBuffer[] = "TANTRAGYAAN";
uint8_t *tx=aTxBuffer;
uint8_t aRxBuffer[16]="";
uint8_t *rx=aRxBuffer;
int main(void)
{
SystemClock_Config();
Configure_GPIO();
Configure_USART();
SendTo_USART();
}
void SendTo_USART(void)
{
for (int index=0; index<11; index++)
{
LL_USART_TransmitData8(USART2,*(tx++));
while (!LL_USART_IsActiveFlag_TXE(USART2))
{
}
}
LL_USART_ClearFlag_TC(USART2);
}
void USART2_IRQHandler ( void )
{
while (!LL_USART_IsActiveFlag_RXNE(USART2))
{
}
if (LL_USART_ReceiveData8(USART2)!='0'||0||"")
{
*(rx++)=LL_USART_ReceiveData8(USART2);
inc=inc+1;
LL_USART_ClearFlag_RTO(USART2);
}
}
void Configure_USART(void)
{
//LL_AHB2_GRP1_EnableClock(LL_AHB2_GRP1_PERIPH_GPIOA);
LL_GPIO_SetPinMode(GPIOA, LL_GPIO_PIN_2, LL_GPIO_MODE_ALTERNATE);
LL_GPIO_SetAFPin_0_7(GPIOA, LL_GPIO_PIN_2, LL_GPIO_AF_7);
LL_GPIO_SetPinSpeed(GPIOA, LL_GPIO_PIN_2, LL_GPIO_SPEED_FREQ_HIGH);
LL_GPIO_SetPinOutputType(GPIOA, LL_GPIO_PIN_2, LL_GPIO_OUTPUT_PUSHPULL);
LL_GPIO_SetPinPull(GPIOA, LL_GPIO_PIN_2, LL_GPIO_PULL_UP);
LL_GPIO_SetPinMode(GPIOA, LL_GPIO_PIN_3, LL_GPIO_MODE_ALTERNATE);
LL_GPIO_SetAFPin_0_7 (GPIOA, LL_GPIO_PIN_3, LL_GPIO_AF_7);
LL_GPIO_SetPinSpeed(GPIOA, LL_GPIO_PIN_3, LL_GPIO_SPEED_FREQ_HIGH);
LL_GPIO_SetPinPull(GPIOA, LL_GPIO_PIN_3, LL_GPIO_PULL_UP);
LL_APB1_GRP1_EnableClock(LL_APB1_GRP1_PERIPH_USART2);
LL_RCC_SetUSARTClockSource(LL_RCC_USART2_CLKSOURCE_PCLK1);
LL_USART_SetTransferDirection(USART2, LL_USART_DIRECTION_TX_RX);
LL_USART_EnableDirectionTx(USART2);
LL_USART_ConfigCharacter(USART2, LL_USART_DATAWIDTH_8B, LL_USART_PARITY_NONE, LL_USART_STOPBITS_1);
LL_USART_SetBaudRate(USART2, SystemCoreClock,LL_USART_OVERSAMPLING_16, 115200);
LL_USART_SetHWFlowCtrl(USART2, LL_USART_HWCONTROL_CTS);
LL_USART_SetOverSampling(USART2, LL_USART_OVERSAMPLING_16);
LL_USART_Enable(USART2);
NVIC_SetPriority(USART2_IRQn, 0);
NVIC_EnableIRQ(USART2_IRQn);
LL_USART_EnableIT_RXNE (USART2);
}
void SystemClock_Config(void)
{
/* MSI configuration and activation */
LL_FLASH_SetLatency(LL_FLASH_LATENCY_4);
LL_RCC_MSI_EnableRangeSelection();
LL_RCC_MSI_SetRange(LL_RCC_MSIRANGE_7);
LL_RCC_MSI_Enable();
while(LL_RCC_MSI_IsReady() != 1)
{
};
/* Main PLL configuration and activation */
LL_RCC_PLL_ConfigDomain_SYS(LL_RCC_PLLSOURCE_MSI, LL_RCC_PLLM_DIV_1, 40, LL_RCC_PLLR_DIV_2);
LL_RCC_PLL_Enable();
LL_RCC_PLL_EnableDomain_SYS();
while(LL_RCC_PLL_IsReady() != 1)
{
};
/* Sysclk activation on the main PLL */
LL_RCC_SetAHBPrescaler(LL_RCC_SYSCLK_DIV_1);
LL_RCC_SetSysClkSource(LL_RCC_SYS_CLKSOURCE_PLL);
while(LL_RCC_GetSysClkSource() != LL_RCC_SYS_CLKSOURCE_STATUS_PLL)
{
};
/* Set APB1 & APB2 prescaler*/
LL_RCC_SetAPB1Prescaler(LL_RCC_APB1_DIV_1);
LL_RCC_SetAPB2Prescaler(LL_RCC_APB2_DIV_1);
/* Set systick to 1ms in using frequency set to 80MHz */
/* This frequency can be calculated through LL RCC macro */
/* ex: __LL_RCC_CALC_PLLCLK_FREQ(__LL_RCC_CALC_MSI_FREQ(LL_RCC_MSIRANGESEL_RUN, LL_RCC_MSIRANGE_6),
LL_RCC_PLLM_DIV_1, 40, LL_RCC_PLLR_DIV_2)*/
LL_Init1msTick(80000000);
/* Update CMSIS variable (which can be updated also through SystemCoreClockUpdate function) */
LL_SetSystemCoreClock(80000000);
}
Please help me.
Thank you.
2018-11-12 1:14 AM
Hi Pavel,
My task is to send some character string from Tx to Rx pin of same USART2. But, to the best of my knowledge, I think that during transmission, only a single character is taken from the string as the TDR register of Tx can hold only 1 byte. So, if I don't use interrupt and send all the characters, then Rx will not be able to sense the incoming characters and I don't see anything being updated in RxBuffer.
I have removed the below line. It was to check whether I am getting any of these characters in 2 subsequent iterations.
if (LL_USART_ReceiveData8(USART2)!='0'||0||"")
I hope my understanding is right and please correct me if I am wrong.
2018-11-12 1:21 AM
I referred the below link:
https://stackoverflow.com/questions/46198829/stm32-hal-usart-receive-by-interrupt
2018-11-12 1:31 AM
Hi waclawek,
I tried setting 4 MHz i.e., LL_RCC_MSIRANGE_6. But again the same problem. But this time the first 2 characters are getting repeated on 11th and 12th position in RxBuffer.
2018-11-12 2:09 AM
Hi All,
When I forcefully assigned the aRxBuffer, like the one shown below, the code worked.
*(rx)=LL_USART_ReceiveData8(USART2);
aRxBuffer[inc]=*(rx);
But I don't understand why it was not taking automatically since rx is defined as pointer to the aRxBuffer.