2015-08-19 10:43 AM
2015-08-19 10:56 AM
Do you have some defines supporting this?
2015-08-19 11:07 AM
Oops, sorry. These are important of course...
---#define
DMA_CHANNEL_USART_TX
DMA1_Channel4
#define
DMA_PRIORITY_USART_TX
DMA_Priority_Low
#define
DMA_COMPLETE_USART_TX
DMA1_FLAG_TC4
#define
DMA_CLEAR_USART_TX
DMA1_FLAG_GL4
#define
DMA_CHANNEL_USART_RX
DMA1_Channel5
#define
DMA_PRIORITY_USART_RX
DMA_Priority_High
#define
DMA_COMPLETE_USART_RX
DMA1_FLAG_TC5
#define
DMA_CLEAR_USART_RX
DMA1_FLAG_GL5
---2015-08-19 11:10 AM
And this perhaps as well for completeness:
#define
LINK_USART
USART1
2015-08-19 12:21 PM
I'd switch the ordering of these
DMA_Cmd (DMA_CHANNEL_USART_RX, ENABLE); DMA_Init (DMA_CHANNEL_USART_RX, &dmaInit);2015-08-19 1:03 PM
Hmm, yes I tried that before and tried it just again with a bit more care. Things are weird.
There seems to be some change, but that is only directly after programming, not after a power cycle. What I find are two differences:After a power cycle it reverts back to the old thing in that I can clearly read from the USART directly but no response at all from the DMA.
BTW here are the byte counts for the DMA:#define
STANDARD_PACKET_SIZE
5
#define
STARTUP_PACKET_SIZE
1
2015-08-19 1:28 PM
- don't look at the USART registers with the debugger (reading the status register by debugger clears the receiver flag and that spoils things for DMA)
- post the relevant DMA registers' content JW2015-08-19 1:45 PM
Thanks for the hint regarding the debugger, particularly for anyone else coming across this conversation. I my case, I am never using the debugger. But just in case reading the memory location at the receive buffer does interfere, I removed that code and I am now just looking at the DMA complete flag. That changed things to the degree that I now get this flag, but just once. This even works after a power cycle.
Real progress, but not quite there yet. Somehow that feels like I am doing something wrong now when it comes to getting the DMA ready for the next go. I'll be poking around that code... To that end one question: Should I set the memory base address each time when I set the DMA byte count? Clearly the byte count gets modified by the hardware as each byte is received. Since it's incrementing the memory address, does that get modified as well? The driver API has not function for that, so the assumption was I didn't need to do that, though I tried it both ways.2015-08-19 2:12 PM
DMA1-ISR gets to 0x00007007 all the time (as far as I can see). I have channel 1 running on the A/D converter for continuous conversion. Once a the beginning it gets to 0x00077007. This is matching hat I am observing otherwise.
2015-08-21 4:49 PM
For the benefit of anyone else coming across this port, it seems the glaring omission was:
RCC_APB2PeriphClockCmd
(
RCC_APB2Periph_AFIO
,
ENABLE
)
;
Though I am not sure why the transmit worked...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.