2011-07-22 6:10 AM
Hello,
I try to write what I receive into a .txt. First I do this: RCC_Configuration(); GPIO_Configuration(); USART_InitStructure.USART_BaudRate = 115200; USART_InitStructure.USART_WordLength = USART_WordLength_8b; USART_InitStructure.USART_StopBits = USART_StopBits_1; USART_InitStructure.USART_Parity = USART_Parity_No ; USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None; USART_InitStructure.USART_Mode = USART_Mode_Rx | USART_Mode_Tx; USART_Init(USARTy, &USART_InitStructure); USART_Cmd(USARTy, ENABLE); USART_SetPrescaler(USARTy, 0x1); USART_IrDAConfig(USARTy, USART_IrDAMode_Normal); USART_IrDACmd(USARTy, ENABLE); I think this is the good configuration (well sure...) then I send the command like this: USART_SendData(USART2, 'a'); then I have tried to do: int size= 128; for (i=0;i<size;i++) { buf[i]= USART_ReceiveData(USART2); fprintf(t1,''%c'',buf); } and I tried to use the USART_Scanf(128); but none of them runs. I don't know how to write into t1, all the text I receive. thanks to any help...2011-08-02 2:48 AM
Ok thanks, I succeed.
But not with the flag TC... I have used a kind of timer for stop the wait if nothing arrive. After this time I leave the loop and thanks to this it runs. Thanks for your help