cancel
Showing results for 
Search instead for 
Did you mean: 

USART HalfDuplex (Rx/Tx) and Rx Funktion

f2
Associate II
Posted on January 27, 2015 at 16:05

Hello,

is it possible to use one USART in HalfDuplexMode (Rx and Tx via Tx Pin) AND the Rx Pin of the same USART to receive another stream?

regards

Florian
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Posted on January 27, 2015 at 17:13

is it possible to use one USART in HalfDuplexMode (Rx and Tx via Tx Pin) AND the Rx Pin of the same USART to receive another stream?

Some how I think it would be very hard to manage, and not lose data.
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
f2
Associate II
Posted on January 28, 2015 at 09:04

Hello Clive,

thank you for the information.

regards

Florian