USART and Hyperterminal
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2013-07-31 2:55 AM
Hi,
I create on my stm3220G evaluation board an example with USART. The code:#include <
stm32f2xx.h
>
#include <
misc.h
> // I recommend you have a look at these in the ST firmware folder
#include <
stm32f2xx_usart.h
> // under Libraries/STM32F4xx_StdPeriph_Driver/inc and src
#include ''stm32f2xx_gpio.h''
volatile char StringLoop[] = ''The quick brown fox jumps over the lazy dog\r\n'';
//**************************************************************************************
int main(void)
{
USART_InitTypeDef USART_InitStructure;
GPIO_InitTypeDef GPIO_InitStructure;
NVIC_InitTypeDef NVIC_InitStructure;
RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOA, ENABLE);
RCC_APB2PeriphClockCmd(RCC_APB2Periph_USART1,ENABLE);
GPIO_PinAFConfig(GPIOA, GPIO_PinSource9, GPIO_AF_USART1);
GPIO_PinAFConfig(GPIOA, GPIO_PinSource10, GPIO_AF_USART1);
/* USART1 Rx */
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_10;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IN;
GPIO_Init(GPIOA, &GPIO_InitStructure);
/* USART1 Tx */
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_9;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
GPIO_Init(GPIOA, &GPIO_InitStructure);
/* Enable USART1 IRQ */
NVIC_ClearPendingIRQ(USART1_IRQn);
NVIC_InitStructure.NVIC_IRQChannel = USART1_IRQn;
NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0;
NVIC_InitStructure.NVIC_IRQChannelSubPriority = 1;
NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;
NVIC_Init(&NVIC_InitStructure);
USART_InitStructure.USART_BaudRate = 9600;
USART_InitStructure.USART_WordLength = USART_WordLength_8b;
USART_InitStructure.USART_StopBits = USART_StopBits_1;
USART_InitStructure.USART_Parity = USART_Parity_No;
USART_InitStructure.USART_HardwareFlowControl = USART_HardwareFlowControl_None;
USART_InitStructure.USART_Mode = USART_Mode_Rx | USART_Mode_Tx;
USART_Init(USART1, &USART_InitStructure);
USART_ITConfig(USART1, USART_IT_TXE, ENABLE);
USART_ITConfig(USART1, USART_IT_RXNE, ENABLE);
USART_Cmd(USART1,ENABLE);
while(1); // Don't want to exit
}
//**************************************************************************************
void USART1_IRQHandler(void)
{
static int tx_index = 0;
static int rx_index = 0;
if (USART_GetITStatus(USART1, USART_IT_TXE) != RESET) // Transmit the string in a loop
{
USART_SendData(USART1, StringLoop[tx_index++]);
if (tx_index >= (sizeof(StringLoop) - 1))
tx_index = 0;
}
if (USART_GetITStatus(USART1, USART_IT_RXNE) != RESET) // Received characters modify string
{
StringLoop[rx_index++] = USART_ReceiveData(USART1);
if (rx_index >= (sizeof(StringLoop) - 1))
rx_index = 0;
}
}
When I use hyperterminal, I don't see anything. why?? I set hyperterminal with the same properties of USART.
THANKS
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2013-07-31 5:00 AM
I create on my stm3220G evaluation board an example with USART. When I use hyperterminal, I don't see anything. why?? I set hyperterminal with the same properties of USART.
Probably because the board uses USART3 on PC10/11?Up vote any posts that you find helpful, it shows what's working..
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2013-07-31 5:25 AM
THANKS clive1. I changed and it works. GPIOC9 RX e GPIOC10 TX.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2013-07-31 5:34 AM
THANKS clive1. I changed and it works. GPIOC9 RX e GPIOC10 TX.
USART3_RX is PC11Up vote any posts that you find helpful, it shows what's working..
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2013-07-31 5:59 AM
I was going to write. But I don't receive anything. Is there a way to send packet to board's usart (for example: length of packet)?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2013-07-31 7:40 AM
I resolve it, but I don't understand. I changed GPIOC11 fromGPIO_Mode_IN toGPIO_Mode_AF and IRQ receive:
from if (USART_GetITStatus(USART3, USART_IT_RXNE) != RESET) to
if (USART_GetFlagStatus(USART3, USART_FLAG_RXNE) != RESET)
what's the difference between
USART_GetITStatus and
USART_GetFlagStatus?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2013-07-31 7:55 AM
Yes, for F2/F4 designs the peripheral pins need to be in AF Mode.
If you want to send/receive multiple bytes you'll need to create some buffering, my preference is for ring/fifo buffers handled under interrupt. The USART has flags in in status register reflecting the state of internal registers and buffers, there is a secondary set of flags related to interrupt enabling, and status. These are covered in the Reference Manual for the parts.Up vote any posts that you find helpful, it shows what's working..