2011-03-14 8:20 AM
I've got STM32F103RET6 chip, 72 MHz, 512K flash and 64K RAM. The chip seems to be pin-to-pin compatible with the STM32F100RBT6.
What if I replace the original chip with this more powerful one? Has anyone ever tried to upgrade the board this way?2011-03-14 9:35 AM
I recently saw the the following on a web site:
''If that isn't enough, just for signing up for the new STM32 design contest, I received a new Discovery module with the STM32F103 chip for free. Same board, but the processor has 1MB of flash, 96K RAM, 72MHz and even more I/O. Yikes! The module isn't for sale yet, nor is the chip, so I don't know the chip or module price. (1/'11)'' This was on the following site: http://www.djerickson.com/stm32/index.html The would be awesome! I love .2011-03-17 8:50 AM
Hi kuchura.yury;
STM32F103RET6 is pin to pin compatible with STM32F100RBT6. You can replace the latter by any STM32 64 pin package.2011-03-24 3:45 PM
Doh! Now I really wish I had signed up for the design contest.
The project I would have used was converting my EV motor controller code. The AVR processor we started with has a slow A/D converter. We do over-current protection in software, and the sample rate isn't high enough to do a good job. There definitely isn't the chance to do waveform reporting, and no compute power left to implement some of the other cool features I wanted to add. One of the interesting features of the controller software is that it does implements automotive OBD-II reporting over CAN, including reporting trouble codes. With the AVR I use a MCP2515 CAN controller over SPI. I was hoping to use the integrated CAN controller on the STLink part of Discovery board, but found that STLink section wasn't really programmable. So instead we continue to use a MCP2515 with the Discovery board. With a little bit of studying i concluded that there were no pin conflicts that would preclude upgrading the main 32f100 to a part with CAN. So I bought a 32f105rct6, planning to solder it in the place of the '100. But I haven't yet been willing to risk breaking a still-working board to do the upgrade.