cancel
Showing results for 
Search instead for 
Did you mean: 

Understanding interruptions

azer asd
Associate II
Posted on October 03, 2017 at 17:54

Hi.

I am currently working with a STM32L476 Discovery board.

I just want to start an interruption handler with a basic timer, but I am facing an issue.

I would like to toggle a LED from the board when the timer is restarting but, for now, the LED doesn't change its state.

It appears that i can go into 'HAL_TIM_PeriodElapsedCallback' but I think this is just for the tick incrementation.

I would like to know why I can't use the handler with my timer.

Thank you for your time.

Here is the code :

uint8_t LCD_String[]= ' STM32L4xx';

GPIO_InitTypeDef s_gpio;

TIM_HandleTypeDef s_timer;

int main(void)

{

    HAL_Init();

  /* Configure the system clock to 80 MHz */

  SystemClock_Config();

  InitializeTimer();

  /* LCD GLASS Initialization */

  BSP_LCD_GLASS_Init();

  Init_GPIO();

    HAL_NVIC_SetPriority(TIM2_IRQn, 0, 0U);

    HAL_NVIC_EnableIRQ(TIM2_IRQn);

  uint_least16_t timer_value;

  unsigned char show_tab[10];

  while(1)

      {

      timer_value = __HAL_TIM_GetCounter(&s_timer);

          sprintf(&show_tab, '%x', timer_value);

          BSP_LCD_GLASS_DisplayString(show_tab);

          HAL_Delay(100);

      }

}

void Init_GPIO()

{

    /*

    * Initialize GPIO for LED4/LED5

    */

    LED4_GPIO_CLK_ENABLE();

    LED5_GPIO_CLK_ENABLE();

    s_gpio.Mode  = GPIO_MODE_OUTPUT_PP;

    s_gpio.Pull  = GPIO_PULLUP;

    s_gpio.Speed = GPIO_SPEED_FREQ_VERY_HIGH;

    s_gpio.Pin = LED4_PIN;

    HAL_GPIO_Init(LED4_GPIO_PORT, &s_gpio);

    s_gpio.Pin = LED5_PIN;

    HAL_GPIO_Init(LED5_GPIO_PORT, &s_gpio);

}

void InitializeTimer()

{

    __HAL_RCC_TIM2_CLK_ENABLE();

    s_timer.Instance = TIM2_BASE;

    s_timer.Channel = HAL_TIM_ACTIVE_CHANNEL_1;

    s_timer.Init.Prescaler = 40000;

    s_timer.Init.CounterMode = TIM_COUNTERMODE_UP;

    s_timer.Init.Period = 500;

    s_timer.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;

    s_timer.Init.RepetitionCounter = 0;

    HAL_TIM_Base_Init(&s_timer);

    /*Starting the timer*/

    HAL_TIM_Base_Start(&s_timer);

}

extern void TIM2_IRQHandler()

{

    HAL_TIM_IRQHandler(&s_timer);

}

void test()

{

    HAL_GPIO_TogglePin(LED4_GPIO_PORT, LED4_PIN);

}

void SystemClock_Config(void)

{

  RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};

  RCC_OscInitTypeDef RCC_OscInitStruct = {0};

  /* MSI is enabled after System reset, activate PLL with MSI as source */

  RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_MSI;

  RCC_OscInitStruct.MSIState = RCC_MSI_ON;

  RCC_OscInitStruct.MSIClockRange = RCC_MSIRANGE_6;

  RCC_OscInitStruct.MSICalibrationValue = RCC_MSICALIBRATION_DEFAULT;

  RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;

  RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_MSI;

  RCC_OscInitStruct.PLL.PLLM = 1;

  RCC_OscInitStruct.PLL.PLLN = 40;

  RCC_OscInitStruct.PLL.PLLR = 2;

  RCC_OscInitStruct.PLL.PLLP = 7;

  RCC_OscInitStruct.PLL.PLLQ = 4;

  if(HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)

  {

    /* Initialization Error */

    while(1);

  }

  /* Select PLL as system clock source and configure the HCLK, PCLK1 and PCLK2

     clocks dividers */

  RCC_ClkInitStruct.ClockType = (RCC_CLOCKTYPE_SYSCLK | RCC_CLOCKTYPE_HCLK | RCC_CLOCKTYPE_PCLK1 | RCC_CLOCKTYPE_PCLK2);

  RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;

  RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;

  RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;

  RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;

  if(HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_4) != HAL_OK)

  {

    /* Initialization Error */

    while(1);

  }

}
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
azer asd
Associate II
Posted on October 03, 2017 at 21:08

The issue was in the NVIC Initialization I the NVIC and Timer into the Initialize_timer :

I think that in the old code I didn't put the 'HAL_TIM_Base_Start_IT(&s_timer);' and maybe the 3 first functions were not in a good order...

void InitializeTimer()

{

    HAL_NVIC_SetPriority(TIM2_IRQn, 10, 0U);

    HAL_NVIC_EnableIRQ(TIM2_IRQn);

    __HAL_RCC_TIM2_CLK_ENABLE();

    s_timer.Instance = TIM2_BASE;

    s_timer.Channel = HAL_TIM_ACTIVE_CHANNEL_1;

    s_timer.Init.Prescaler = 0x1FFF;

    s_timer.Init.CounterMode = TIM_COUNTERMODE_UP;

    s_timer.Init.Period = 0XFFF;

    s_timer.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;

    s_timer.Init.RepetitionCounter = 0;

    HAL_TIM_Base_Init(&s_timer);

    /*Starting the timer*/

    //HAL_TIM_Base_Start(&s_timer);

    HAL_TIM_Base_Start_IT(&s_timer);

}

emalund
Associate III
Posted on October 03, 2017 at 21:12

I am not going to muddle through your code, but if the LED changexs between on and off more then ~10 times / second it will appear not to change