Skip to main content
Uwe Bonnes
Chief
January 27, 2015
Question

Unbonded GPIO pins

  • January 27, 2015
  • 1 reply
  • 497 views
Posted on January 27, 2015 at 15:00

What happens with unbonded GPIO pins with chips packaged in a package where not all pins fit. With all families beside L0, default GPIO setup is input mode. Floating inputs in this configuration may result in unwanted current surge.

Should unbonded GPIO pins be treated as floting pins or does the chip itself care for these unbonded pins?
    This topic has been closed for replies.

    1 reply

    Danish1
    Lead III
    January 27, 2015
    Posted on January 27, 2015 at 17:21

    If you set all unbonded pins to be ANALOG inputs then the digital input circuit will be disabled and you won't suffer class-A leakage current.

    One rival manufacturer I know about had all pins (that can be analog) power-up as analog, so pretty much the first problem a newbie user hits is that they can't make digital inputs work!