cancel
Showing results for 
Search instead for 
Did you mean: 

Unavailable (per package) pin state

Austin Glaser
Associate
Posted on October 06, 2015 at 01:54

What's the best state to put GPIOs which aren't connected to a pin on a particular package in? Does it make any sort of difference? I'm concerned primarily with power consumption.

Thanks in advance!
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Nesrine M_O
Lead II
Posted on October 06, 2015 at 10:47

Hi glaser.austin,

By default, STM32F4 pins are configured as inputs, except some JTAG pins which can impact the power consumption of the device in different power modes because 

pins are very sensitive to external noise in input mode I/O. To avoid extra I/O current, all pins should be configured as analog input (AIN); in this mode the 

Schmitt trigger input is disabled, providing zero consumption for each I/O pin.

I'd highly recommend you to have a look to this

http://www.st.com/web/en/resource/technical/document/application_note/DM00096220.pdf

 that gives a measuring application that can be customized to measure the current consumption 

of different STM32F4 power modes, and shows how to best configure the system for each mode.

-Syrine-