2017-07-07 5:43 AM
Hi,
could you help me please to implement reading registers from USB ULPI chip ?
thanks for all replies
Kind regards ...
2017-07-07 7:27 AM
AFAIK there's no provision for direct access (read nor write) of ULPI registers available in the HS_OTG in STM32.
Disclaimer: I don't use the HS_OTG.
JW
2017-07-07 7:37 AM
i'm trying to solve my issue:
https://community.st.com/0D50X00009XkiVqSAJ
and i got idea to read ULPI's registers as basic testcase of communication ... i don't need to read registers during running state ... sufficient for me is to read ULPI vendor id for example and confirm regarding docs ...
2017-07-07 10:44 AM
Bitbang the ULPI protocol?
Sounds like a challenge for real men... should be doable if the PHY's clock can be turned to input...
JW
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.