Skip to main content
Alex Fedoseev
Associate II
August 6, 2017
Question

Typo in UM1670

  • August 6, 2017
  • 1 reply
  • 815 views
Posted on August 06, 2017 at 21:35

There seems to be a typo in UM1670 -  Discovery kit with STM32F429ZI MCU, Section 6.7. (TFT LCD).

It says 'The STM32F429ZIT6 controls this motion sensor through the SPI interface.'  But it talks about ILI9341 LCD controller, witch is NOT a motion sensor. Yes, ILI9341 can be controlled via SPI, but its performance is better when used on LTDC. This line seems to be a copy-paste typo from the section above that talks about gyroscope mems and IS NOT the best representation of ILI9341.

#stm32f429-disco
This topic has been closed for replies.

1 reply

Amel NASRI
ST Technical Moderator
August 8, 2017
Posted on August 08, 2017 at 12:07

Hi

Fedoseev.Alexand

‌,

Thanks for highlighting this typo. It will be fixed in coming UM version.

-Amel

To give better visibility on the answered topics, please click on "Best Answer" on the reply which solved your issue or answered your question.