2009-12-16 05:04 AM
Trouble with USB_EPxR
2011-05-17 04:34 AM
(Performance, not connectivity line USB interface.)
I’ve been having trouble loading the USB_EPxR registers. No matter what I do either in my assembly code or with my yellow J-Link-ARM debugger the registers always show zero. When I plug in a USB cable my ISR handler is called, so I can’t be that far off base. Doubtless, I am missing something. I hope it’s my software and not my STM3210E-EVAL board. I’ve had no problems with ADC/DMA and timer to trigger conversions so the board can’t be seriously broken. What could cause these registers to be unsettable?