cancel
Showing results for 
Search instead for 
Did you mean: 

Trouble with one VDD pin of STM32F103

Paul Andreev
Associate II
Posted on June 08, 2018 at 09:15

I use STM32F103CBT6 for my project. This is something trouble this time. One of VDD pins of MCU is broken and not have connection to pcb. Another three pins are fine. Would MCU work fine if i not resoldering it and working current is low? I test two different VDD pins of STM32 with multimeter. Seems pins internally connected.

#stm32f103 #vdd-pin #stm32
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
AvaTar
Lead
Posted on June 08, 2018 at 10:44

Not sure if you get a satisfying answer, only ST's design engineers are supposed to know.

I would at least avoid getting this chip in customer's hands.

Even if connected, different VDD pins might supply different regions of the silicon. Bonding wires use to be quite thin. Perhaps you might experience trouble under high load conditions with low supply voltage.

Posted on June 08, 2018 at 11:11

Thx, i think just resolder chip to avoid future troubles.