touch issue with STM32f303
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2019-10-30 4:31 AM
Hi all,
STM32F303 is as capability to sens touch which is surface touch principal . I am trying to get the values on STM studio but unfortunately i am not able to see any values on it. there always a flat line. I am posting my code can anyone tell me what I am doing wrong.
Because on hardware side these is only 1 register which is on series. apart from that everything is take care by touch library.
any kind of suggestion would be helpful
Thanks in advance
#include "main.h"
#include "touchsensing.h"
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_TSC_Init(void);
/* USER CODE BEGIN PFP */
tsl_user_status_t tsl_status;
void switch_test(void);int main(void)
{
/* USER CODE BEGIN 1 */
/* USER CODE END 1 */
/* MCU Configuration--------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* USER CODE BEGIN Init */
/* USER CODE END Init */
/* Configure the system clock */
SystemClock_Config();
/* USER CODE BEGIN SysInit */
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_TSC_Init();
MX_TOUCHSENSING_Init();
/* USER CODE BEGIN 2 */
/* USER CODE END 2 */
/* Infinite loop */
/* USER CODE BEGIN WHILE */
while (1)
{
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
tsl_status = tsl_user_Exec();
if (TEST_TKEY(1)){
HAL_GPIO_WritePin(LED1_GPIO_Port,LED1_Pin,1);
}
else{
HAL_GPIO_WritePin(LED1_GPIO_Port,LED1_Pin,0);
}
}
/* USER CODE END 3 */
}
/**
* @brief System Clock Configuration
* @retval None
*/
void SystemClock_Config(void)
{
RCC_OscInitTypeDef RCC_OscInitStruct = {0};
RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
/** Initializes the CPU, AHB and APB busses clocks
*/
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE;
RCC_OscInitStruct.HSEState = RCC_HSE_ON;
RCC_OscInitStruct.HSEPredivValue = RCC_HSE_PREDIV_DIV1;
RCC_OscInitStruct.HSIState = RCC_HSI_ON;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE;
RCC_OscInitStruct.PLL.PLLMUL = RCC_PLL_MUL9;
if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
{
Error_Handler();
}
/** Initializes the CPU, AHB and APB busses clocks
*/
RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
|RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV2;
RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;
if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_2) != HAL_OK)
{
Error_Handler();
}
}
/**
* @brief TSC Initialization Function
* @param None
* @retval None
*/
static void MX_TSC_Init(void)
{
/* USER CODE BEGIN TSC_Init 0 */
/* USER CODE END TSC_Init 0 */
/* USER CODE BEGIN TSC_Init 1 */
/* USER CODE END TSC_Init 1 */
/** Configure the TSC peripheral
*/
htsc.Instance = TSC;
htsc.Init.CTPulseHighLength = TSC_CTPH_2CYCLES;
htsc.Init.CTPulseLowLength = TSC_CTPL_2CYCLES;
htsc.Init.SpreadSpectrum = DISABLE;
htsc.Init.SpreadSpectrumDeviation = 1;
htsc.Init.SpreadSpectrumPrescaler = TSC_SS_PRESC_DIV1;
htsc.Init.PulseGeneratorPrescaler = TSC_PG_PRESC_DIV4;
htsc.Init.MaxCountValue = TSC_MCV_8191;
htsc.Init.IODefaultMode = TSC_IODEF_OUT_PP_LOW;
htsc.Init.SynchroPinPolarity = TSC_SYNC_POLARITY_FALLING;
htsc.Init.AcquisitionMode = TSC_ACQ_MODE_NORMAL;
htsc.Init.MaxCountInterrupt = DISABLE;
htsc.Init.ChannelIOs = TSC_GROUP1_IO4;
htsc.Init.ShieldIOs = TSC_GROUP2_IO4;
htsc.Init.SamplingIOs = TSC_GROUP1_IO3|TSC_GROUP2_IO1;
if (HAL_TSC_Init(&htsc) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN TSC_Init 2 */
/* USER CODE END TSC_Init 2 */
}
/**
* @brief GPIO Initialization Function
* @param None
* @retval None
*/
static void MX_GPIO_Init(void)
{
GPIO_InitTypeDef GPIO_InitStruct = {0};
/* GPIO Ports Clock Enable */
__HAL_RCC_GPIOC_CLK_ENABLE();
__HAL_RCC_GPIOF_CLK_ENABLE();
__HAL_RCC_GPIOA_CLK_ENABLE();
/*Configure GPIO pin Output Level */
HAL_GPIO_WritePin(LED1_GPIO_Port, LED1_Pin, GPIO_PIN_RESET);
/*Configure GPIO pin : LED1_Pin */
GPIO_InitStruct.Pin = LED1_Pin;
GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
HAL_GPIO_Init(LED1_GPIO_Port, &GPIO_InitStruct);
}
/* USER CODE BEGIN 4 */
/* USER CODE END 4 */
/**
* @brief This function is executed in case of error occurrence.
* @retval None
*/
void Error_Handler(void)
{
/* USER CODE BEGIN Error_Handler_Debug */
/* User can add his own implementation to report the HAL error return state */
/* USER CODE END Error_Handler_Debug */
}
#ifdef USE_FULL_ASSERT
/**
* @brief Reports the name of the source file and the source line number
* where the assert_param error has occurred.
* @param file: pointer to the source file name
* @param line: assert_param error line source number
* @retval None
*/
void assert_failed(char *file, uint32_t line)
{
/* USER CODE BEGIN 6 */
/* User can add his own implementation to report the file name and line number,
tex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
/* USER CODE END 6 */
}
#endif /* USE_FULL_ASSERT */
/************************ (C) COPYRIGHT STMicroelectronics *****END OF FILE****/
Labels:
- Labels:
-
STM32F3 Series
-
TSC
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0