Skip to main content
mattgczapar
Associate
October 17, 2011
Question

TotalFifoSize in STM32f107

  • October 17, 2011
  • 0 replies
  • 409 views
Posted on October 17, 2011 at 17:52

I have been looking at the USB OTG Libraries for the 105/7 and I've come across the variable  TotalFifoSize.  It's set to 320, when using the Full speed core.

I was wondering if anyone knew if this was because of a hardware spec, that I can't seem to find, or if it is a choice made by the libraries, and if it is a choice, what are some of the reasons one might consider when making that choice.

The value is set to 320 in the file usb_core.c around line 234. 

snippet of usb_core.c:

.....

 /* initialize device cfg following its address */

  if (coreID == USB_OTG_FS_CORE_ID)

  {

    baseAddress                = USB_OTG_FS_BASE_ADDR;

    pdev->cfg.coreID           = USB_OTG_FS_CORE_ID;

    pdev->cfg.host_channels    = 8 ;

    pdev->cfg.dev_endpoints    = 4 ;

    pdev->cfg.TotalFifoSize    = 320; /* in 32-bits */

    pdev->cfg.phy_itface       = USB_OTG_EMBEDDED_PHY;     

    ....
    This topic has been closed for replies.