cancel
Showing results for 
Search instead for 
Did you mean: 

Too Slow TFTP transfer speed

mrniknejad
Associate II
Posted on May 17, 2013 at 07:13

Hi All 

I am using TFTP example in my project using STM32F2x7_ETH_LwIP_V1.1.0  library but my problem is about the transfer speed !! my results explain that a 255KB file transfer from Pc to ARM take about 3 minutes to complete and its awful for me.

so is there any way to increase the transfer speed ?

thanks

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
amin23
Associate II
Posted on May 17, 2013 at 17:25

Hi,

I think the application takes a large amount of time to write the file into the SD card and not in the transfer. so the majority of time is spent in the writing process

mrniknejad
Associate II
Posted on May 18, 2013 at 21:26

No i don't think so, because the writing speed in SD card is so much faster than that ! 

to ensure about that i comment the write function in SD and the result is the same and make no difference in transfer speed !!!!

Posted on May 18, 2013 at 22:22

The throughput suggested seems very low.

Depending on the block size, a Class 10 SDHC card can be 6-7 MBps writing, 18-19 MBps reading. The SDIO implementation on the F2/F4 isn't too bad, the SPI of the F107 is a bit sluggish, but would still expect 200-300 KBps.

I guess I'd be looking at the Ethernet side of things, checking buffers, timeouts and such. Might want to snoop the traffic, see what's going on.
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..