cancel
Showing results for 
Search instead for 
Did you mean: 

TIMPRE HCLK multiplier in F413

Bob Anderson
Associate
Posted on May 17, 2018 at 11:08

In RM0430 rev 7 section 6.2 it is stated that when TIMPRE is set and APB prescaler is 1 or 2 then the timer clock is HCLK.

And when APB prescaler is > 2 then the timer clocks are HCLK * 4.

This is different to the F446 which in RM0390 section 6.2 which states that when APB prescaler is > 4 then timer clocks will be HCLK * 4.

So is the F413 indeed different as stated in the RM or is this a typo in the RM and the F413 is the same as the F446?

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Imen.D
ST Employee
Posted on May 17, 2018 at 15:49

Hello

Anderson.Robert.002

,

The F413 and

F446

products are different regarding this point and thereference manuals are correct.

In fact, t

he maximum

HCLK frequency and the maximum APBs frequencies are not the same.

With Regards,

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen
Bob Anderson
Associate
Posted on May 17, 2018 at 16:06

Hi Imen.

Thanks for the confirmation.

Also another question will the next update of the Cube Eclipse plug-in implement the TIMPRE setting so that the clock configuration has the correct timer clocks when TIMPRE is set?

Thanks,

Bob