2010-03-30 9:28 AM
Timer values determination question...
2011-05-17 4:45 AM
This should work for a 72 MHz system clock.
-Clive TIM_TimeBaseInitTypeDef TIM_TimeBaseStructure; u16 x; // Period, interrupt periodicity in timer ticks u16 y; // Prescale another clock divider (1-65536) int TIM3_Frequency; RCC_ClocksTypeDef RCC_ClockFreq; // APB1 has a max speed of 36 MHz, with 72 MHz system clock a /2 divisor is used. // x = 4500; y = 8; // x = 7200; y = 5; x = 1000; y = 36; // Clock at 1MHz, 1000 ticks, 1 KHz RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM3, ENABLE); /* Time base configuration */ TIM_TimeBaseStructure.TIM_Period = (x - 1); TIM_TimeBaseStructure.TIM_Prescaler = (y - 1); // 1-65536 TIM_TimeBaseStructure.TIM_ClockDivision = TIM_CKD_DIV1; // 1,2 or 4 for tDTS TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up; TIM_TimeBaseInit(TIM3, &TIM_TimeBaseStructure); /* TIM IT enable */ TIM_ITConfig(TIM3, TIM_IT_Update, ENABLE); /* TIM2 enable counter */ TIM_Cmd(TIM3, ENABLE); NVIC_InitTypeDef NVIC_InitStructure; NVIC_InitStructure.NVIC_IRQChannel = TIM3; NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 1; NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0; NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE; NVIC_Init(&NVIC_InitStructure); RCC_GetClocksFreq(&RCC_ClockFreq); TIM3_Frequency = (RCC_ClockFreq.PCLK1_Frequency / y) / x; // APB1 (TIM3) printf(''TIM3 Interrupt rate %d Hz\n'',TIM3_Frequency);2011-05-17 4:45 AM
>>APB1 has a max speed of 36 MHz ...
This is true, but remember that the clock signal which is presented to the timers TIM2-TIM7 might be twice the APB1 clock (72 MHz) - if the APB1 prescaler is anything but 1. See the ''clock tree'' in RM0008.2011-05-17 4:45 AM
Indeed, my bad.
-Clive x = 1000; y = 72; // Clock at 1MHz, 1000 ticks, 1 KHz .. RCC_GetClocksFreq(&RCC_ClockFreq); if (RCC_ClockFreq.HCLK_Frequency == RCC_ClockFreq.PCLK1_Frequency) TIM3_Frequency = RCC_ClockFreq.PCLK1_Frequency; else TIM3_Frequency = RCC_ClockFreq.PCLK1_Frequency * 2; TIM3_Frequency = (TIM3_Frequency / y) / x; // APB1 (TIM3) printf(''TIM3 Interrupt rate %d Hz\n'',TIM3_Frequency);2011-05-17 4:45 AM
Hi all,
thanks for the reply. So the values you have for ''X'' and ''Y'' are for 1KHz or can I plug in any values? I ran the program with your settings, and I'm seeing approx 9ms transition time... So what would be the values for 1hz? I ended up with 132 for period, and (72000000/1200)-1 for prescaler (59999) How were those numbers derived? I got them from a sample... Again, I really appreciate the help and am trying to understand!2011-05-17 4:45 AM
Hi all,
Okay, does this formula work? == setup == sysclock = 72,000,000 tim_counter_clock = 24,000,000 freq = 36,000 duty = 2 (1=100%, 2=50%, 3=33%, 4=25%, etc) TIM_Period (TIMx_ARR) = (tim_counter_clock / freq) -1 Prescaler (TIMx_PSC) = (sysclock / tim_counter_clock) -1 TIM_Pulse (TIMx_CCRx) = (Prescaler / duty) TIM_Period (TIMx_ARR) = (24,000,000 / 36,000) -1 = 2 Prescaler (TIMx_PSC) = (72,000,000 / 24,000,000) -1 = 666 TIM_Pulse (TIMx_CCRx) = (666 / 2) = 333 (50%) now the key is keeping the values at 16bit, so I would need to adjust my ''tim_counter_clock'' Does this sound reasonable?2011-05-17 4:45 AM
>>thanks for the reply. So the values you have for ''X'' and ''Y'' are for 1KHz or can I plug in any values?
Generally speaking I would keep the Y (prescaler) value as small as possible to keep the granularity of the 16-bit timer ticks as small as possible, while keeping X under 65536. I'd pick a value that makes the math easy, so dividing the clock by 10, 36 or 72. >>I ran the program with your settings, and I'm seeing approx 9ms transition time... I'm not using it to generate pulses, but rather interrupts. The interrupt rate matches the rated printed (by the 2nd corrected fragment), and was compared against a 1000 Hz (1ms) SYSTICK timer. >>So what would be the values for 1hz? I ended up with 132 for period, and (72000000/1200)-1 for prescaler (59999) With a TIMCLOCK of 24 MHz, x = 50000, y = 480, I have a 1 second interrupt. >How were those numbers derived? Simple division. Base on the source clocks. ((240000000 / 480) / 50000 = 1 -Clive