cancel
Showing results for 
Search instead for 
Did you mean: 

Timer pulse of period 10 microseconds(4 microseconds delay + 1 microsecond pulse + 5 microseconds delay)

saimaddy123
Associate II
Posted on June 02, 2011 at 05:18

Hi,

I would like to generate a timer pulse of period 10microseconds, where first 5 microseconds is LOW and then a pulse of width 1 microsecond followed by 5 microseconds LOW again. 

I looked at examples in ST library like one pulse, external Trigger synchronization etc. They do not appear to fit what I want. Could any one throw any ideas on how this can be done?

Sai

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Posted on June 02, 2011 at 17:46

Not sure if you want one shot, or repetitive.

SPI in slave mode you can drive the clock, and shift arbitrary patterns, with a controlled frequency/period. The ST part is less flexible than most (8 and 16 bit only). For your pattern shifting at 8 MHz might be viable. If the SPI was programmable for 10 bit you could have used 1 MHz clock.

Pattern generation could also be achieved by DMAing to a GPIO port. Clocked via a timer set to 1 MHz
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..